You are here: Tools > Human Machine Interface Editor > Create a New Controller

Using Kollmorgen Visualization Builder

To work with Kollmorgen Visualization Builder, do as follows:

Create a new controller

This procedure is applicable when you use Kollmorgen Visualization Builder externally.

Import variables into the project

When you open the Kollmorgen Visualization Builder with your KVB panel (by double-clicking the KVB panel from the project explorer) all the variables tagged into the Dictionary are automatically imported into Kollmorgen Visualization Builder. Once the file is imported, all PLC variables are available for use within Kollmorgen Visualization Builder.

Design the Panel

Add Object

You can drag-and-drop predefined objects from the library to the screen. The library is located in the Home tab of Kollmorgen Visualization Builder.

Customize Object

Select an object and click the General tab to customize:

Map Variable to the Object

In the General tab, you can set the Variable or Tag that maps to the current object in the Tag/Security section.

Download the Panel

To download your panel you have to use the Project ribbon in Kollmorgen Visualization Builder that contains the Transfer command .

Command

Description

Validate

Compiles the project to check for errors

Run

Validates the program, runs it on the development computer and communicates with the PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system

Simulate

Validates the program, runs it on the development computer, but does not communicate with the PAC

Transfer (1st icon)

Is for projects with a dedicated HMI device (AKI)

Validates the current project and sends it to the selected hardware

Transfer (2nd icon)

Validates the project and saves it to a folder with an executable program that can be run on a PAC with the HMI runtimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running (Visualizer RT) installed or a dedicated HMI panel

How to download on the HMI device (AKI)

To download you must be connected directly to the HMI panel through an EthernetEthernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs) cable. As the IP address is already defined (for more details, Configure the Controller), nothing special has to be done before transferring your panel to the graphic operator terminal.

How to download on the PAC (AKC)

Related Documents

For further information on Kollmorgen Visualization Builder, refer to the following manual:

KVB Guide   Description
Kollmorgen Visualization Builder™ Quick Start Guide Quick Start that covers the most important points to install and use Kollmorgen Visualization Builder, in order to configure HMI Panels and PCPersonal Computer operated control applications, including applications for PACs
Kollmorgen Visualization Builder™ User Manual Contains all the content to help you with Kollmorgen Visualization Builder

Concept Link IconSee Also

 

Create a New Controller

Import Variables into the Project

Design the Panel

Dowload the Panel


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™